Industry Online Support
Technical Forum
2/26/2013 11:32 AM | |
Posts: 3037 Rating: (192)
|
Hello, Can you describe more what you do? Can you post a screenshot? Which panel do you use? Do you have check if another application use the COM1? Tweety |
2/26/2013 12:37 PM | |
Posts: 13 Rating: (0) |
hello , thank u Mr Tweety for replay, i have protool pro/cs V6.0 + sp3, widows xp sp3, just i don't have com port com on my lapetope (dell inspron6400), so can i simulate without port com1? |
Last edited by: tarik147 at: 2/26/2013 8:23 PM |
|
2/26/2013 8:21 PM | |
Posts: 13 Rating: (0) |
And i want simulate OP7 , just for information, don't have this problem with wincc v7.0.1 or wincc flexible Runtime, |
2/27/2013 6:14 PM | |
Posts: 3037 Rating: (192)
|
Hello, You need a real serial interface for project transfer to an OP7. "Real" interfaces are interfaces without implementation via USB. This means that you cannot use any "USB to serial" adapter. What transfer options are available in the various operator panels? Tweety |
2/28/2013 1:57 PM | |
Posts: 13 Rating: (0) |
thankx a lot |
Follow us on