Industry Online Support
Technical Forum
3/7/2013 11:33 AM | |
Posts: 14 Rating: (0) |
look how is value of QW80 in online mode |
3/7/2013 11:44 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, In hardware configuration for that module is possible to be assigned: 1. +-10V this correspond to-27,648 to 27,648 2. 0-20mA corresponding to0 to 27,648. Then download the hardware copnfiguration. The CPU is in RUN mode (assumed the module is correct hardware connected). Please clarify on which module's pins do you measure (current or voltage). Connection diagram can be find inhttp://support.automation.siemens.com/WW/view/en/36932465(from 316th page). Best regards, Hristo Mihalev |
3/7/2013 1:40 PM | |
Posts: 9 Rating: (0) |
The module was defect, PLC program said the module was missing or removed when using hardware configuration, when it infact was in the slot |
Follow us on