Industry Online Support
Technical Forum
2/27/2013 1:44 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, The 200 is a small PLC with onboard I/0, the 300 series is used for bigger machines 256 i/O on the main rack possible. I would not go for the 200, because it can be over with this type of CPU any day, a good replacement would be the S7- 1200. I think your ptogram will even fit in a LOGO, to test it you can download the Logosoft Demo and see if it is good enough for your needs. Regards, Marcjan |
Problem solved? |
|
3/3/2013 7:58 PM | |
Posts: 8946 Rating: (999) |
You will be happy with a S7-1200. The Logo! is not a good solution, i am afraid. |
3/4/2013 9:34 AM | |
Posts: 8946 Rating: (999) |
Also, the 1200 CPU is nearly same price like Logo! but much more possibilities. |
Follow us on