3/16/2013 12:48 PM | |
Joined: 9/27/2006 Last visit: 9/20/2024 Posts: 12282 Rating: (2684)
|
Hello freeze; Extension racks can be connected to the central rack of the SA7-300 CPU with 2 technoogies. Your choice will depend on how many racks you need to connect, how far they are located from the CPU, and what else you want to connect on the remote "racks". The basic premise is that you will need an interface module (IM xxx) to connect any remote rack. 1) If the distance between the CPU on the central rack is very short (inside the main cabinet for example) then you would select either an IM 365 or an IM 360/IM 361 pair. - the IM 365 is a unit consisting of 2 modules (one Send, one Recieve) attached by a one meter cable; you place the Send moduleto the right of the CPU in the main rack, the Recieve module at the head of the remote rack (if you have only IO modules you do not need a power supply, power will be supplied by the central rack CPU) and you setup the remote rqack to a maximum distance of one meter. You can have a single remote rack (8 more modules)attached to the IM 365. - the IM 360, setup also to the immediate right of the CPU in the cetral rack, can connect to an IM 361 in a remote rack at a maximum distance of 10 meters (cable to be purchased seperately); also the IM 361 can connect to another one in another remote rack, altogeteher one IM 360 can connect to 3 IM 361s, so you can connect to (4 x 8 modules/rack) 32 S&-300 IO modules in all. You will find a complete description on these IMs in the following manual for the S7-300 modules, in chapter 8, Interface modules. SIMATIC S7-300 S7-300 Module data SIMATIC Distributed I/O device ET 200M |
Last edited by: dchartier at: 3/16/2013 2:35 PMLast edited by: dchartier at: 3/16/2013 2:34 PM |
|
This contribution was helpful to2 thankful Users |
3/16/2013 2:51 PM | |
Joined: 9/27/2006 Last visit: 9/20/2024 Posts: 12282 Rating: (2684)
|
Hello freeze; If you mean using Profibus-DP, it is recommended to use Profibus-DP certified cables and connectors, especially if you are using this in an industrial settingwhere you want to ensure correct communication links. You will find a lot of information on Siemens Profibus equipment here: SIMATIC NET PROFIBUS Networks
|
Last edited by: dchartier at: 3/16/2013 3:08 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on