Industry Online Support
Technical Forum
3/28/2013 9:27 AM | |
Posts: 61 Rating: (0) |
Hello everyone, I'm stuck so I need your help. Little description about program: Pressing the START push button, line with boxes start moving. When the sensor for boxes registers 1 box, line stops, and the line with apples starts. Once sensor for apples counted 10 apple, line for apples stop moving and system restart and start all over again. System will stop working if I push STOP button. I'm stuck I don't know how to repeat system. In attachment I'm sending my file and pic. If someone have a better idea or advise how to create this please let me know, becouse I'm new in this and I will gladly take ideas/advices. Best regards, Goran AttachmentOB1.pdf (54 Downloads) |
3/28/2013 10:20 AM | |
Posts: 61 Rating: (0) |
Here is program that is working in simulator, so please can someone look at digram and tell me is this correct and is there another way to do it ?
AttachmentOB1_v2.pdf (52 Downloads) |
3/28/2013 11:07 AM | |
Posts: 366 Rating: (30) |
Hy please try my examples in attachment. I have used markers instead of in-/outputs. But i think you can read the code. nice regards AttachmentFC70.pdf (52 Downloads) |
This contribution was helpful to1 thankful Users |
3/28/2013 11:08 AM | |
Posts: 366 Rating: (30) |
also the symbols |
This contribution was helpful to1 thankful Users |
Follow us on