4/17/2013 10:41 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
Hello, not all DQ Connection use the 24V The grey data cables which delivered with the DQ components have no 24V connector pins. The 24V pins normaly use to connect SMI modules or DQ Encoders which get the power 24V with the DRIVE-CLiQ interface. Line- ande Motormodules get the 24V power from the front connector. But the DQ connection are wired as Cross Connect Ethernet Cable, so if you use a normal patch ethernet cable (1:1) then it can be misfunction. Regards Christoph |
Follow us on