6/10/2007 3:20 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi, Normally the programs that use EPROMs are called COM-packages, you may find on the internet the checkpage where all COM-packages are checked Executability of COM Packages Under STEP 5/ST V7.1x. When you use only STEP5 for the EPROM and you may chose the right one then that is ok, when you can not chose however the EPROM that you have, then don't try to shoot the EPROM with that version. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
6/11/2007 7:39 AM | |
Posts: 3 Rating: (0) |
Hi, Dear Late ; Yes, I got it completley what you mean Thanks a lot , best wishes |
Last edited by: arash at: 11.06.2007 07:41 |
|
Follow us on