5/5/2013 11:08 PM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of the User Engineer Ghulam
|
5/6/2013 1:39 PM | |
Joined: 8/31/2010 Last visit: 4/14/2024 Posts: 1509 Rating: (222) |
Hello Engineer Ghulam, Each screen takes a screen number by default which can also be altered. Now your job is to make use of this system function ActivateScreenByNumber. The trick here is you have to create a tag 'ScreenNumber' of data type INT (for example). Under the value change event of that ScreenName tag add this system function ActivateScreenByNumbermentioning the ScreenNumber tag as Screen_number parameter. Now when you change the screen number tag from your PLC for the said time intervals, this in turn changes the desired screen from your PLC. Hope this helps. |
Like it? Rate it! |
|
Follow us on