5/2/2013 7:25 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello, I think that is OK, check it online before assign the parameter to timer. Variable Time Value Timer
Integer vale to S7 time format conversion[code] L MW 100 // Integer contains secondsITD L L#1000 *D // Time equivalent T #z CALL "TIM_S5TI" // time to s5 timer conversion IN :=#z RET_VAL:=MW102 // s5 timer data type[/code] Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 5/2/2013 7:27 AM |
|
This contribution was helpful to1 thankful Users |
5/2/2013 7:34 AM | |
Posts: 515 Rating: (56) |
Hi raffi, To achieve this you can use a real data type in the SCADA, convert it to time using the "Real to Time" block(FC18) and further to s5 time using FC40. Kindly find the attached document for your reference please
AttachmentReal to Time1.pdf (2123 Downloads) |
5/2/2013 7:53 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello shazin, It is a bit OFF-TOPIC because we talked about INT to TIME conversion.The point is , In which library we should search for FC18 you mentioned?More complex issue discussed here! Best regards Hamid Hosseini |
This contribution was helpful to1 thankful Users |
5/2/2013 9:39 AM | |
Posts: 515 Rating: (56) |
Hi Hamid Hosseini, I am sorry if my post was irrelevant for you.
|
5/2/2013 2:50 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello friends,
This topic is discussed here and I hope proposed solution is helping there.
We all here willingly check new ideas even they are OFF-TOPIC with complete details.In your excerpt of codes (from a real machine) FC18 is a missing point. A snapshot of the "properties"of that function may give us more information like what I have done for FC40(form IEC library in STEP 7). Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 5/3/2013 4:34 PM |
|
Follow us on