1/6/2012 7:40 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello It seems only one of the Indexes in the Combo Box can be connected to a String Tag If you attach a Dynamic Tag to The Index Text to any Index then is is shown for all indexes. ( Athough in runtime it only works for the index for thich it was defined ) Attaching more than one text to seperate Dynamic Tags does not work. I wonder if this is a bug or Delibrate Or am i missing something !! Navnag |
Last edited by: Navnag at: 1/11/2012 2:23 PMLast edited by: O_Moderator at: 1/10/2012 12:25 PMnew subject after splitting from /tf/WW/en/Posts/52995#top There is no such thing as the last bug in a program |
|
1/12/2012 1:34 PM | |
Posts: 1776 Rating: (95)
|
Hi, well that´s a bug. Please contact Siemens customer support with a support request. |
This contribution was helpful to1 thankful Users |
6/5/2013 9:50 AM | |
Posts: 11 Rating: (0) |
Hi Navnag, Did you have a solution from Support? İf you had ,please tell me ok. similar problem I have too. Thanks |
Follow us on