6/18/2013 9:26 AM | |
Posts: 87 Rating: (0) |
Hi, I have CPU Module 6AA6-504-0AA. I don't have a manual. Can someone help me please? |
6/19/2013 2:39 AM | |
Joined: 10/7/2005 Last visit: 4/24/2024 Posts: 3004 Rating: (1046) |
Hello Sasongko your 6AA6504-0AA is indeed a valid part part number, albeit one that belongs to the SICOMPMMC216 product family. While it looks similar to an S5 system and S5 I/O's could be used with it, it is a product family in its own right. I do unfortunately not have any manualsfor it and as it it is rather ancient gear and there is also very little info available for it on the web. I suggest you get in touch with your local Siemens rep and asked him to see who from Siemens AG may be the right person to talk too and perhaps still has harcopies of the orginal manuals that could be scanned. Ideally though, you get rid of it and upgrade the system to an S7. I hope this helps |
Cheers |
|
This contribution was helpful to2 thankful Users |
Follow us on