6/25/2013 11:23 AM | |
Joined: 3/14/2008 Last visit: 9/24/2024 Posts: 2096 Rating: (938) |
Hello, some guys here put a picture window in the @screen picture, so in case a tag is written, the pop up will show at any screen which is opened. Last week it was suddenly gone, and figured someone runned project editor so the default screen is set back... In project editor I cannot exclude the @screen.pdl from being updated (in tab: General data). I can however set the @screen as read only, so I won't be updated, but warnings will pop up during compilation...etc.. Is there any other way to display the picture window at any screen? Putting in the picture window at each picture is a lot of work... PCS7 6.1 sp4 thxxx |
If I could help you, you can use the RATE button. Thank you. |
|
6/25/2013 11:57 AM | |
Joined: 3/14/2008 Last visit: 9/24/2024 Posts: 2096 Rating: (938) |
That one is being changed as well... I can change the default picture in the base pool directoy (where wincc is installed in C:/program files..... but when there is an update to new version, the file is changed again.Not so neat... |
If I could help you, you can use the RATE button. Thank you. |
|
6/25/2013 3:40 PM | |
Joined: 3/14/2008 Last visit: 9/24/2024 Posts: 2096 Rating: (938) |
TerminalBuzz, Didn't know what the *peep* you meant, but i looked into the sample cfg file. In there I edited some settings and created my own layout, its working like a charm.. Thanks for the info, didn't know you could create your own layouts like that. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on