6/26/2013 5:30 PM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477)
|
How you are connecting to drive? If you are trying to connect from PLC, you have to set gate wayfor this Have a look at following http://support.automation.siemens.com/WW/view/en/49229556 /tf/WW/en/Posts/30664 And for direct connection, you must have drive - pc connection kit or you must use PG Also try using search function, you can find lot of discussion of how to be online with drive using starter or scout Regards, Devesh |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
6/27/2013 10:34 PM | |
Joined: 2/3/2011 Last visit: 9/5/2024 Posts: 348 Rating: (10) |
I´m using CP5611 in Profibus, I attached the image of parameters. And connected in DEVICE access point. Thanks. |
Follow us on