Industry Online Support
Technical Forum
7/2/2013 3:00 PM | |
Posts: 767 Rating: (69) |
Hello tementaXCD, I am not aware of anybody being successful in the general type of description you provide for an application. Limitations which come to mind: 1. A servo drive for a servo motor regulates the phase angle for optimum commutation of its pulse width modulated output waveform to optimize amount of torque for rotation of motor(resulting in movement of load). I am not aware of any microcontroller which can perform this optimum commutation. 2. Concerning positioning to close the position loop must have some type of feedback to a device which can provide position feedback either to servo drive or to micro controller. In many servo drive systems the servo drive can interpret the feedback from servo motor and monitor /perform position commands. For instance, SINAMICS S110 drive or SINAMICS S120 drive systems with SIMOTICS S-1FK7 servo motors. Size of motor needed would depend upon the mechanics of transfer motor rotation to movement of load. On the other hand for position regulation, a true monitoring could be performed by an external encoder providing feedback to to microcontroller Else, a crude positioning could be performed by use of limit switches to a digital input. Following is link toCAD Creator which has information on motors, SINAMICS S110, and SINAMICS S120 drive systems. http://staging04.it-motive.de/CADCreator/VorNavigation.cfm?IdListVornavi=(0-1*906)&CFID=3839767&CFTOKEN=81272061&Scenario= Attached is a brochure for SINAMICS S120 AC Drive, which would primarily consist of Power Module, CU310-2 controller, servo motor, power cable, and feedback cable. Primary difference for SINAMICS S110 drive is that the controller would then be a CU305 controller instead of CU310-2 controller. Best Regards, Deputy AttachmentJ:\1.Public\Product_Information\15. SINAMICS\Brochure\Brochure - SINACMICS S120 Single Axis AC Drive.pdf (321 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on