Industry Online Support
Technical Forum
7/2/2007 11:50 AM | |
Posts: 37 Rating: (0) |
Hello everybody We are on the phase on making a new plant,I am attaching here the automation network layout of the plant. My concerns: 1-which is better ,connecting the 2 servers on a ring network with the S7-400 PLCs as shown on the layout ,or connecting the 2 servers and the PLCs on a star topology?I mean in terms of reliability,stability. 2-is the place of the engineering station is correct on the network?...I beleive that it has to be on the ring network. Thank you Attachmentnetwork.pdf (418 Downloads) |
7/2/2007 1:05 PM | |
Posts: 1776 Rating: (95)
|
Hi, see the following FAQ: http://support.automation.siemens.com/WW/view/en/21456821 Best regards April |
7/2/2007 1:49 PM | |
Posts: 37 Rating: (0) |
Thanx ................But can I get an answer for my second questions regarding the engineering stations? |
7/3/2007 9:56 AM | |
Posts: 1776 Rating: (95)
|
Hi, You do Right. You need Access to ring, cause You need it for Access to automation Bus. Its shown in slide 14 in the above pdf Best regards April |
7/4/2007 4:13 PM | |
Posts: 37 Rating: (0) |
Thank you very much April. But,if we connect the ES as on my network layout will work or not? Regards |
Follow us on