Industry Online Support
Technical Forum
6/30/2013 10:30 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello, I do not want to repeat what friends already said here... But SIEMENS alredy have comptability tool and also a pdf file that contains the comptability table for WinCC flexible (all versions). The above entry is updated on 13/5/2013 It's not mentioned there that WinCC flexible is comptable with MS Windows 7 Home edition. And it's very strange to know from some people here that they already installed WinCC flexible on Windows 7 Home! Why SIEMENS did not put MS Windows 7 Home in the list?!! And from few days in another thread, another member told that he already installed it on Windows 8. And Also SIEMENS do not put Windows 8 in the list!! I have never tried it on Windows Home. And I do not like to try... In my opinion the best way to work is to see which software you need and see which recent OS is comptable with all of them. So, if it's already comptable, I hope that SIEMENS will add MS Windows 7 to the list. And also if you have a look on oredering description ofWinCC flexible 2008, You will found: WINCC FLEXIBLE 2008 ADVANCED ENGINEERING-SW,FLOATING LICENSE LICENSE KEY ON USB STICK, SW AND DOCUMENTATION ON DVD IN GER/EN/IT/FR/SP/CHS/CHT/KOR/JPN EXECUTABLE UNDER XPPROF/ WINDOWS7 PROFESSIONAL/ULTIMATE/ ENTERPRISE (32/64 BIT), FOR CONFIGURATION OF SIMATIC PANELS AND WINCC FLEXIBLE 2008 RUNTIME |
Last edited by: Ayman Elotaify at: 6/30/2013 10:31 PMAyman Elotaify |
|
This contribution was helpful to1 thankful Users |
Follow us on