7/8/2013 11:50 PM | |
Posts: 109 Rating: (11) |
Yes it will need drivers Also have a look at few more adapters in attachment AttachmentUSB_RS232_Adapter_en_V1_2.pdf (521 Downloads) |
7/9/2013 5:35 AM | |
Posts: 47 Rating: (8) |
Hi Friendz, Look the above desired MLFB i.e. 3UF7946-0AA00-0 comes with a small CD containing its driver. First load it to your PC and then use is it accordingly. But I would like to recomment you a new MLFB i.e. 3UF79410AA000 which is launched in AUG' 2012. With this MLFB you can connect your Simocode, 3RK MSS & 3RW Softstarters directly from device to PC via USB. Well, i am suggesting you this becuase you are yet to buy any product at this moment. AttachmentActual pic.pdf (306 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on