7/9/2013 7:42 AM | |
Joined: 10/3/2010 Last visit: 3/14/2024 Posts: 1552 Rating: (188) |
Hey 42752071 thanks for your update, I guess we misunderstood your issue but it's clear now. Which Office version do you have? What is your exact WinCC Version 6.2? SP3 with or without hotfixes? maybe check hotfixes for possible fixes Also check your WinCC diagnose directory for possible errors in log files. If nothing else can be found, try to uninstall Configuration Tool and re-install it. I've been using Configuration Tool since WinCC V7, never had that problem. |
Last edited by: SteBo at: 7/9/2013 7:53 AMLast edited by: SteBo at: 7/9/2013 7:51 AMB r g d s , |
|
This contribution was helpful to1 thankful Users |
7/9/2013 10:50 AM | |
Posts: 12 Rating: (0) |
TanksSteBo, My Office is 2003,Simatic Wincc V6.2 sp3 ASIA K6.2.3.0 I can't find thesuspicious error in log files. I am not uninstall or reunstall the soft, I am afraid thesystem breakdown,you know I will use Wincc V7 in the next project.
|
7/9/2013 11:00 AM | |
Joined: 10/3/2010 Last visit: 3/14/2024 Posts: 1552 Rating: (188) |
TanksSteBo, My Office is 2003,Simatic Wincc V6.2 sp3 ASIA K6.2.3.0 I can't find thesuspicious error in log files. I am not uninstall or reunstall the soft, I am afraid thesystem breakdown,you know I will use Wincc V7 in the next project. K6.2.3.0 means that no hotfix is installed while most recent hotfix is already Hotfix 14 (released on 2012-05-24). It is possible that this "bug" is anyway solved by implementing a hotfix. Maybe you can try to create a new project from start, just to check the same behaviour or not in a new project or does your last reply means that this topic has to be considered as closed? |
B r g d s , |
|
7/9/2013 3:23 PM | |
Posts: 12 Rating: (0) |
K6.2.3.0 means that no hotfix is installed while most recent hotfix is already Hotfix 14 (released on 2012-05-24). It is possible that this "bug" is anyway solved by implementing a hotfix. Maybe you can try to create a new project from start, just to check the same behaviour or not in a new project or does your last reply means that this topic has to be considered as closed? But the same problem.I will reinstall the Windows and all of the soft next time.
|
Follow us on