Industry Online Support
Technical Forum
7/1/2013 7:27 PM |
|
Posts: 54 Rating: (3) |
Thank youSteBo all your replies helped me a lot bt still I will be posting the detailed screen shots and the other informations in details. Regards -pk2_kdh
|
7/3/2013 7:21 AM | |
Posts: 54 Rating: (3) |
dearAmit_86 i will be shortly posting the screen shots . now one of my systems i have found that same bt two types of licences are there and I guess that due to two licences the message is coming... now how to delete the unused one. it is not getting deleted by normal option. - pk2_kdh
|
7/3/2013 7:26 AM | |
Posts: 39 Rating: (1) |
Dear pk2_kdh your question is not clear . Please make it clear. |
7/3/2013 7:37 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello, Thanks for update. Please post the screenshot as soon as you get it. I also suggest you do one thing if you cannot delete the License from Automation License Manager. Simply Connect USB Pen drive to PC & transfer the unwanted license to that USB Stick. Siemens USB Stick is generally preferred to transferred the license back to Pen drive. Also, you can delete the trial license from your Hard disk. from "AX NX ZZ Folder". it will be hidden folder so you have to make it visible. Be careful!!!!!! if you delete the license make sure that it is expired trial license. please donnot delete any Similar original license and transfer it to USB Stick. Hope it helps. |
VANDE MATARAM..... |
|
7/3/2013 7:42 AM | |
Posts: 54 Rating: (3) |
Dearcorleone U please go through the complete set of posts and view the replies. It may clear it out the problem in details. I am stating the same again. 1st: inspite of giving original licences and that also in drive C the licence pop up comes. 2nd: only single licences are there. 3rd: it is not that licences are conflicting 4th: when I am checking the licences via automation licence manager it is showing "OK" and "used" also go through the folowing link which may help u. In any case, follow instruction here to avoid this pop up message again: - pk2_kdh
|
7/3/2013 7:53 AM |
|
Posts: 54 Rating: (3) |
dearAmit_86 ok I will be doing this using one fresh pen drive and will update the status. But why it is not deleting from the normal delete option..? - pk2_kdh
|
7/3/2013 9:13 AM | |
Posts: 39 Rating: (1) |
thank you pk2_kdh it helped me a lot.. |
This contribution was helpful to1 thankful Users |
7/10/2013 6:48 PM | |
Posts: 54 Rating: (3) |
dear corleone did u get what my question is..? are there any doubts remaining? then feel free to ask. - pk2_kdh
|
Follow us on