4/27/2009 4:01 PM | |
Posts: 33 Rating: (0) |
Thanx IsabelS, I think I know what you mean (must be the logical device name mentionned above). I will try some things later and post here again ;) |
4/28/2009 11:14 AM | |
Joined: 4/5/2006 Last visit: 9/16/2024 Posts: 917 Rating: (63) |
Hi markiii, if you are able to connect with plc from VM means your TCP/IP configuration should be wrong. Check your TCP/IP "system parameters", you have to select the right network card here. In "Connection Properties" you have to be sure to insert CPU rack & slot (not CP, often guys insert wrong data here). In attachment 2 bmp Regards AttachmentWinCC 7 with VM.zip (376 Downloads) |
7/12/2013 4:24 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
New question splitted to S7 installed in VM, unable to connect to the LAN Best regards O_Moderator |
Follow us on