6/26/2013 5:13 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Hello, Please have a look at nice example from Pegia. The S7-200 CPUs have high speed counters incorporated to do this task. The conversion counting pulses to frequency, however, must be done by user software. How to calculate frequency from counting pulses measurement Hope this helps. |
VANDE MATARAM..... |
|
7/15/2013 6:29 AM | |
Posts: 461 Rating: (29) |
Hi all, Sorry for my very late reply because of another assignment,still i finished this on saturday... I just finished this by means of using HSC with the use of proximity sensor & also there s some change in motor spec, at first the sensor was not able read the pulses correctly then i changed the sensor based on SolutionFinder statement on selecting the sensor, switching frequency of sensor must be higher than the switching frequency at your maximum speed. Now i was able to read the pulses properly Thanks & Regards, Nelliyan.G |
This contribution was helpful to2 thankful Users |
7/15/2013 1:54 PM | |
Posts: 559 Rating: (87) |
Thanks for the update. |
7/16/2013 6:55 AM | |
Posts: 461 Rating: (29) |
My pleasure |
Follow us on