Industry Online Support
Technical Forum
7/24/2013 3:20 PM | |
Joined: 9/27/2006 Last visit: 4/17/2024 Posts: 12256 Rating: (2664) |
Hello Krsh; To clear up any misunderstanding, you have to understand that Global Data exchanges is atechnical word in S7 CPUs for smalldata exchangesover MPI (serial comms). See the following FAQ for a few more details: Basic communication between CPUs with global data So when you started your thread with CPU-to-CPU communications and inserted the words Global Data you triggered a lot of immediate responses on MPI comms. Please make sure you give the specifics of the question you are asking (in this case, Ethernet exchanges between CPUs) in order to avoid such misunderstandings. Hope thois helps, Daniel Chartier |
7/25/2013 10:17 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
New question was splitted to Is it possible to communicate with Rockwell PLC Compact Logix L45 via INAT Ecochange Gateway with CPU-315 2PNDP (V3.2.7) on profinet port?. Best regards O_Moderator |
This contribution was helpful to1 thankful Users |
Follow us on