7/26/2013 9:25 AM | |
Posts: 28 Rating: (5) |
Hi rogabob, can you explain what do you want to do with AO ? since you wrote that you send data to the OPC server and then to LabView, i think you can do that without really turn on the PQW just write the value in the PLC's memory and then send it, but if you want to load value to PQW, hope this attachment can help you, but you also need to make sure you wire the analog output correct before , regards Shaumi AttachmentB2-analog processing.pdf (180 Downloads) |
7/26/2013 11:36 AM | |
Posts: 9 Rating: (0) |
used L 27648 T PQW 754 and got 10V. I didn't know how to use L and T. sorry it was my first experience with AO and AI. |
7/27/2013 8:49 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi rogabob, Anweisungsliste (AWL) für S7-300/400 - Siemens Industry Online ... |
7/29/2013 2:13 PM | |
Posts: 9 Rating: (0) |
sorry for my back^) Is it possible to set AO in 2,6V? Or how to calculate L? |
7/29/2013 2:51 PM | |
Joined: 9/27/2006 Last visit: 5/10/2024 Posts: 12257 Rating: (2666)
|
Hello rogabob; |
Last edited by: dchartier at: 7/29/2013 3:10 PM |
|
Follow us on