7/24/2013 11:26 AM | |
Joined: 3/24/2010 Last visit: 7/29/2024 Posts: 118 Rating: (1) |
Kindly see the attached data block for your reference. I made some screenshots of the Data block parameters online. Regards, Daniel AttachmentSiwaM_DB_Page1to3.zip (165 Downloads) |
7/24/2013 2:17 PM | |
Posts: 206 Rating: (22) |
Hi Cyborg, you are aware that the Siwarex M is outdated? The successor of it is the Siwarex FTA, see www.siwarex.com . If you want to start a dosing you have to send the set point (DR22) and the dosing data (DR23) which includes the tolerances, switching values and settling time.In the manual http://support.automation.siemens.com/WW/view/en/7787784 Chapter 3.9 – 3.11 you find a description of the dosing functions.If you have started the dosing you should see the signal “proportioning running” in DR31 Status 2. There you also find the coarse and fine signals and the tolerance signals. Regards ABenno |
Last edited by: ABenno at: 7/24/2013 2:18 PM |
|
7/25/2013 11:04 AM | |
Joined: 3/24/2010 Last visit: 7/29/2024 Posts: 118 Rating: (1) |
Hello , Please find the attached screenshots of my Data block. Regards, Cyborg AttachmentSiwarex M_DB.zip (163 Downloads) |
7/31/2013 9:30 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
New question was splitted to upgrade weighers which uses siwarex M and is now defective Best regards O_Moderator |
Follow us on