3/3/2013 7:56 PM | |
Posts: 8946 Rating: (999) |
Yes!
No, failsave and ex are complete different things! |
3/4/2013 7:45 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
http://support.automation.siemens.com/WW/view/en/14198947 and many more links just use search option here in forum. Best regards, Hristo Mihalev
|
7/8/2013 7:21 AM | |
Joined: 8/27/2006 Last visit: 4/23/2024 Posts: 719 Rating: (88) |
Ex modules are intended to be mounted inside hazardous areaswhere there is possibility for explosion because of the availability of flammable gas in the air, so if a module outputs a tiny spark, the whole place could go down. So Ex modules are certified to produce very little current so that it is not enough to create a spark. Failsafe modules and programming blocks are certified for failsafe operation and that's mainly intended for critical processes where double checking for instruments and output signals is essential.
|
The more you know, The more you know that you don't know |
|
This contribution was helpful to1 thankful Users |
7/9/2013 7:37 AM | |
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating: (9) |
Ex modules are intended to be mounted inside hazardous areaswhere there is possibility for explosion because of the availability of flammable gas in the air, so if a module outputs a tiny spark, the whole place could go down. So Ex modules are certified to produce very little current so that it is not enough to create a spark. Failsafe modules and programming blocks are certified for failsafe operation and that's mainly intended for critical processes where double checking for instruments and output signals is essential. By Ex modules you mean Intrinsically safe modules right? |
8/12/2013 11:46 AM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
Follow up question published by Ziemensis split to a seperate thread with the subject Simatic s7 failsafe - catalog pdf for failsafe components. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on