Industry Online Support
Technical Forum
1/16/2012 12:53 PM | |
Joined: 4/5/2006 Last visit: 4/24/2024 Posts: 917 Rating: (63) |
Hi Nil96,
PCS7 connection with AS400-H is possible with CP16x3 only; by redconnect is possible to configure redundant connection in Netpro without addition effort by developer. Follow the link of previuos Tread with same topic Redundant connection between PLC and WinCC Redundant connection plc <-> WinCC Follow a link that explain why you shouldn't have the wizard in WinCC Explorer (you don't need maybe...just in case? Some time i see the option "create redundant connection" in dynamic wizard window and some time it disappears Hope can help regards |
1/18/2012 12:06 AM | |
Posts: 71 Rating: (12) |
Also can we use teaming between 2 different card manufacturers ?? Maby it is possible but I don't think that is a good Idea. Please, get more specific on the Communication / Networks forum I think "teaming" option is with Intel NIC cards. Plz correct if I am wrong !! I'm not sure that I understand the question but for example I used Broadcom Netxtreme cards with teaming. There are lot of venodors wich provides hardware with a teaming option. |
9/3/2013 5:49 PM | |
Joined: 4/21/2006 Last visit: 4/16/2024 Posts: 510 Rating: (24) |
New question was splitted to a new thread: connect quantum DCS (2 redundant quantum CPU's) with WinCC thr... |
Follow us on