9/1/2013 2:42 PM | |
Posts: 47 Rating: (0) |
Hello Experts, My machine is having following drive sections with profibus control 1. UE module _6SN1145-1AA01-0AA2 2. Spindle drive_6SN123-1AA0-0DA2, 6SN1118-1NH01-0AA1 3. Oscillator drive_6SN123-1AA0-0BA1,6SN1118-1NH01-0AA1 The machine is running 3years. Recent days only we are facing following alarm in Spindle drive A149 : Incorrect data for modulo axis with absolute encoder, Supplementary info 49 or 50 or 84. Anyone tell me how to solve the issue permanently, what are the possible causes? Note: Every time we are referencing the axis. UE module output voltage 579 VDC. Drive parameter file attached. Regards, Uthaya AttachmentDrive 12A - Station 2 Spindle.zip (194 Downloads) |
Follow us on