7/24/2013 8:21 AM | |
Joined: 7/8/2012 Last visit: 1/24/2024 Posts: 40 Rating: (0) |
Hello, I create a one project in Wincc Flex as opc server and another project as a Client.
When I put wincc Flex OPC server in RUNTIME i can access the all the Tags in Client project. But when I am trying to connect Wincc as a OPC client and Red Lion as a OPC server. I have created OPC server with 3 tags. This 3 tags access with another OPC client Successfully. When I am trying to connect with wincc flex then OPC server showing Connected and running status. But i am unable to browse tag from OPC server in Wincc Flex. also i am trying to Connect s7-200 PC Access with Wincc Flex Same thing is happenning. Please help me as early as possible. AttachmentRED LION ERROR.pdf (72 Downloads) |
7/24/2013 9:58 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147)
|
Hello amsd, Here is a link to manual: SIMATIC HMI WinCC flexible 2008 Communication Part 1 See chapter 4 And perhaps this link might help: how do you configure the OPC server PC Access in order to operate WinCC flexible Runtime as OPC client? Best regards, Wizard |
7/26/2013 1:20 PM | |
Joined: 7/8/2012 Last visit: 1/24/2024 Posts: 40 Rating: (0) |
I read the manual and done setting as per given but unable to browse tag. I have also access all the configured tag on Elipse scada but unable to access on Wincc Flex Please help me on this.
|
7/26/2013 3:12 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147)
|
Hello amsd, Ok, strange. Please download latest update for WinCC flexible 2008 SP3: Update for WinCC flexible 2008 Service Pack 3 Install and try again. Best regards, Wizard |
7/27/2013 1:31 PM | |
Joined: 7/8/2012 Last visit: 1/24/2024 Posts: 40 Rating: (0) |
[quote user="Wizard"]Hello amsd, Ok, strange. Please download latest update for WinCC flexible 2008 SP3: Update for WinCC flexible 2008 Service Pack 3 Install and try again. Best regards, Wizard Dear Wizards, I have checked on OPC scout i can see configured tags. I will download the updates and will try to browse tag. Regars, amsd |
Follow us on