7/19/2011 2:22 PM | |
Posts: 9 Rating: (0) |
Dears hi I hope you are happy and in good health I get problem during downloading to the CPU 417-4 v5.0 ERR1 :( the number of communication jobs (1800) configured in your program exceeds the maximum permitted number of communication jobs (1200) of the connected CPU) But the limitation of configuration in communication resources (CPU properties) IS 3000 And this type of the CPU can set up to 10000 communication jobs I try to make a full download to check if that can help 1-Download to HW config (and I check the communication job is 3000) 2- Download to the Net pro 3- Entire compile of the selected CPU (here I get warning but no err) W1: The PO UPDAT (cf279) not the last block in OB100 W2: In ob100 there 1347 block /runtime group/ SFC charts installed this is can lead to problem when compiling with SCL compiler W3: In ob 32 there is 558 block /runtime group/ SFC charts installed this is can lead to problem when compiling with SCL compiler 4- Entire downloads to the selected CPU (SE-05) The result is CPU cancels the downloading after delete all the data block function block and we lost the program from the memory card of the CPU I try to repeated downloading (CFC) it finish and ok I expect the problem is solved I make a little change in one CFC chart after that I compile it as changes Gave the warning W1: The PO UPDAT (cf279) not the last block in OB100 no ERRS I tray to download the changes again I get the same problem ERR1 :( the number of communication jobs (1800) configured in your program exceeds the maximum permitted number of communication jobs (1200) of the connected CPU) How the massage come and I check in the static of chart references the communication jobs reach 1800 and still under the CPU setting Splitted from Communication Jobs. |
Last edited by: CS Moderator at: 7/19/2011 7:58 PMnew subject after splitting |
|
9/17/2013 12:05 PM | |
Posts: 15 Rating: (1) |
Thats solve my problem thanks... |
Follow us on