10/6/2013 1:59 PM | |
Posts: 30 Rating: (0) |
Hi all, i have problem with logo display :( in simulation everything working but when i record program in to LOGO (OBA6) does not work correct. I set in text message ON/OFF for marker and if in simulation activated normaly show on the display but no correct show on logo display :( check program. THX.
AttachmentProjekt1_test.zip (191 Downloads) |
Last edited by: PeTer111122 at: 10/6/2013 2:02 PM |
|
10/9/2013 8:26 AM | |
Posts: 30 Rating: (0) |
Hi Helmut_13 i have question it is possible assign to the counter any text on the TD display with LOGO! OBA6. For exam: i want show message to operator on display which program is adjustment. I set program with BCD pulse and calculate with counter which combination is adjusted. I want show on display no nummber but only text for example M14. ( Number 1 is Lietsse, number 2 is M14 and number 3 is Din.) It is possible??
Attachmenttest_prog.zip (174 Downloads) |
10/9/2013 9:49 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, You can do it but not with one counter, you need some more. See example attached. Regards, Marcjan Attachmentchange_text_counter.zip (189 Downloads) |
Problem solved? |
|
This contribution was helpful to1 thankful Users |
10/9/2013 4:28 PM | |
Posts: 2930 Rating: (432)
|
Hi, back to your first question about the status text. You want to use a dig. flag to show a status text. As I mentioned a LOGO! 0BA6 doesn't supprot the dig. flag to trigger the status text. If you don't use all supported outputs of LOGO! 0BA6, then you can use one of the un-used outputs for the status text. Attached is an example how it works with an un-used output. To control an output with LOGO! you do not have wired/used in your machine is no problem for LOGO!. Hope this helps AttachmentStatustext un_used Q.zip (187 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on