10/2/2013 2:10 PM | |
Posts: 16 Rating: (0) |
I suggest you contact Kessler.
Tel: +49 (0) 7582 809-180 |
10/16/2013 12:44 PM | |
Joined: 11/26/2006 Last visit: 3/13/2024 Posts: 36 Rating: (5) |
Two weeks later :) Machine is now in working condition,and from two days produce details. I have received answer from Kessler company,and it's very useful. There is it.(see attachment) And there is info about same motor from Heidenhain "Motor.mot" table. Hope it can help to somebody who is in my position before :) TYPE ASM NAME DMS100.AL.4.FOS-D1932 MODE 0 I-N 44,0 U-N 210 N-N 1100 F-N 39 U0 190 I0 26,4 R1 165 R2 127 Xstr1 228 Xstr2 275 XH 4364 N-XH 4000 N-FS 2040 N-MAX 12000 %XH 150 %K100 PZ 2 TK 0,0037 STR256 SYS6 Dir + TMax150 IMax 70,4 P-N10000 J0,032 Attachment000_101_536-D1932-Deckel,Pfronten.pdf (378 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on