Industry Online Support
Technical Forum
10/24/2013 6:05 AM | |
Posts: 3 Rating: (0) |
Hi , I wonder if this is the right place to post. I have an opposite problem, while trying to import SCD file (which I created from SEL Architect) to Digsi 4.87 (IEC61850 Ed2), I am getting following errors. I have checkedthe scd filewith IEC browswer. Can anyone pleasehelp me with this? // List header // ActionDateTime ------------------------------------------------------------------------------------------ The SCD file is invalid.2013-10-2416:56:15 It does not correspond to the XML scheme of IEC61850-Part 6. It is therefore not possible to import it. The XML validation tool detects the following errors: Error at file C:\SCD\SEL_SCD.SCD, line 16837, char 39 Message: element 'EnumType' declares duplicate identity constraint unique values Import failed!2013-10-2416:56:15 Action completed - 3 fault(s), 0 warning(s)2013-10-2416:56:15 ------------------------------------------------------------------------------------------ Thanks, Aman AttachmentSEL_SCD.zip (197 Downloads) |
Last edited by: O_Moderator at: 10/24/2013 8:44 AMnew subject after splitting from /tf/WW/en/Posts/96355#top |
|
10/24/2013 10:46 PM | |
Posts: 3 Rating: (0) |
Thanks Mike, Using Ed 1 gives an error saying "the specified import file has a different IEC61850 Edition than th ereceiving station". Regards, |
Follow us on