Industry Online Support
Technical Forum
10/31/2013 9:11 AM | |
Posts: 21 Rating: (0) |
Motor: Oriental Motor (Model PK296-03B) Driver: CSK series CSD2145P Hi all, I am trying to move the stepper at different speed values (10 RPM and 20 RPM speed selectionusing toggle switch). I have written a ladder logic using PTO/PWM wizard to get the same. The program works well for 10 RPM, but when selected 20 RPM it takes 1pulse per second. I am attaching the program with this thread as I am unable to figure out mistakes in it (my limitation). Kindly help me troubleshooting it. In future I would like to improve the same program for any speed value. I want to use two push buttons (Increase/decrease) which will change the speed by 1 RPM every time they are pressed. Any help is appreciated. Thanks. Arihant AttachmentCW+CCW.zip (69 Downloads) |
Follow us on