10/30/2013 4:52 AM | |
Joined: 8/25/2006 Last visit: 4/18/2024 Posts: 2203 Rating: (277)
|
Hello. Which versions of software you are using now (Step7, CFC, D7-SYS)? Check them for compatibility.
Did you try complete reinstallation of all Siemens software with registry cleaning like mentionedhere?
Did you change the CPU in HWConfig in current project?
Did you try to connect without any third-party adapter, i.e. directly using MPI or Ethernet?
Did you try to select DUST1 in 'Set PG/PC Interface'? If it will not work also (could not be selected), there is a possibility to select DUST1 for all D7-SYS programs independently of settings in 'Set PG/PC Interface'. For this run the program C:\Program Files\Siemens\Step7\S7BIN\p7sdonlx.exe and select COM1 or COM2, then try to download via DUST1. To change back the selection of online interface run this program again and select 'PG/PC'. Anyway it looks like you have some problems with the project files (if you could go online with other FM458-1DP from other project). Did you try to make a copy of your current project using 'Save as... With reorganization (slow)' in Simatic manager? |
11/1/2013 9:00 AM | |
Posts: 8 Rating: (0) |
Hello KSN, after reading your post, I found the Siemens compatibility tool (thank you for mentioning that), and checked the whole config. Because I use an XP SP3, I downloaded the Step7 v5.4 SP5 package from Siemens, installed it, and now - theoretically - I am a bit closer to the solution. I could download the FM458 program using D7load and RS232 connection to the FM (the MPI connection is still unselectable in Simatic Manager) but there is some trouble: - the EXTF LED on the CPU is on but it can be switched into RUN state - the INTF LED on the FM is on, unit remained in STOP, restart was unsuccessful - the HW diag reports that the FM is unavailable - in CPU error buffer, there are two kind of messages about the FM (i.e. event 3 and event 10, see attachment); it seems that it cannot be known as FM458 although the correct order number appears in the hardware config (and that has been downloaded into the CPU more times), and it is plugged into slot 16 as projected How is it possible that a module with the right order number (checked on its faceplate) and placed in the correct (expected) slot cannot be seen by the CPU normally? Attachmentdiag.zip (146 Downloads) |
11/1/2013 10:21 AM | |
Joined: 8/25/2006 Last visit: 4/18/2024 Posts: 2203 Rating: (277)
|
Hello. Step7 5.4 SP3 could work with D7-SYS 6.2 SP3, but you can't install DUST1. I think with Step7 5.4 SP5 is the same situation. To install DUST1 you need HF3 for D7-SYS 6.2 SP3.
D7-Load is old program. Did you look at the followingFAQ? I'm not sure that you have properly loaded the program.
Did you try to make a copy of project using'Save as... With reorganization (slow)'?
I think this is possible besause of you still didn't load the program to the FM, program inside FM is not running.
|
Follow us on