10/25/2013 7:13 AM | |
Posts: 93 Rating: (2) |
Hi All, We are trying to establish communication with MAG8000-RS485 MODBUS RTU Card without success. We connected MODBUS Cards Tx, RX, Com Ports with Modbus cable to RS485 to RS232 converter. Then following are the different tries we did: A: Communication with Modscan32 software. We set all preconfigured parameters same as default of MODBUS card. Selected MODBUS RTU only as it doesn't support any TCP/ASCII. So, I thought it should work. Unfortunately, message displayed on it as " Device Not Connected". B: Then I tried to establish the communication with PDM and did the following steps to communicate over PDM: 1. Opened SIMATIC Manager. 2. Insert "Modbusnet" on net. 3. Define the properties of my PCs Com Port (1) Settings and Baud Rate (19200). 4. Define the properties of Modbus net, Setting of Comport, Baud Rate, Even, 1 stopbit. 5. Insert "Modbus device" on Modbusnet. Assign MAG8000 Basic. Named it MAG8000 Basic. 6. Upload the data from Device to PC/PG. 7. It this moment, it shows in progress followed by message: "Communication: Process Device not found." Screenshots of MODBUS with Simatic PDM.pdf attached for your review. C: Then I thought it could be problem due to RS485-RS232 conversion, so I directly took it over to Honeywell RTU with which we are going to integrate it with MAG8000. We took it directly over to RS485 Card no conversions but again "Bad Communication"-on. I'll attach screenshots in next msg. AttachmentMODBUS with Simatic PDM.pdf (348 Downloads) |
10/25/2013 7:15 AM | |
Posts: 93 Rating: (2) |
screen shots of honeywell communication is aattached here for review, Looking forward to recieve positive feedback, Regards, Davinder Singh AttachmentHONEYWELL HC900 CONTROLLER.pdf (331 Downloads) |
11/22/2013 10:00 AM | |
Joined: 2/17/2011 Last visit: 1/18/2024 Posts: 4 Rating: (0) |
my personal modbus test software but in chinese. AttachmentC:\Users\cn1yq190\Desktop\PI3Modbus_openby7z.001.zip (310 Downloads) |
Last edited by: Zhou at: 11/22/2013 10:13 AM |
|
11/22/2013 10:12 AM | |
Joined: 2/17/2011 Last visit: 1/18/2024 Posts: 4 Rating: (0) |
change name like zip.002 andput it in a foldertogether with the other two. AttachmentC:\Users\cn1yq190\Desktop\PI3Modbus_openby7z.002.zip (289 Downloads) |
11/22/2013 10:15 AM | |
Joined: 2/17/2011 Last visit: 1/18/2024 Posts: 4 Rating: (0) |
change name like zip.003 andput it in a foldertogether with the other two. AttachmentC:\Users\cn1yq190\Desktop\PI3Modbus_openby7z.003.zip (312 Downloads) |
Follow us on