11/18/2012 2:52 PM | |
Joined: 11/15/2012 Last visit: 8/29/2024 Posts: 143 Rating: (8) |
Greatings to all! I am using step 7 5.5 and simatic net 2010 on my win7. Sometimes I resume my notebook from sleep, I got a error as the attachment shows. It happens random andreally annoying, as it keeps coming out andsystemlevel error. Software I installed on my win7 Ultimate 32bit with UAC open: Step 7 5.5 pro(No SP installed) WinCC Flexible 2008 sp2 (No Update installed) Simatic Net 2010 Some FM software packages like fm350-X etc. I searched the siemens website, found a solution for step 7 5.5 sp2, in step 7 5.5 there is no such tab. And the pniopcac.exe is from Simatic Net rather than step7. Please some good guys provide the right solution. Thank you all! https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=61595882&caller=view |
11/18/2012 3:13 PM | |
Joined: 11/15/2012 Last visit: 8/29/2024 Posts: 143 Rating: (8) |
the pniopcac.exe is from simatic net not from the step7 |
11/18/2012 6:14 PM | |
Joined: 8/25/2006 Last visit: 9/18/2024 Posts: 2209 Rating: (278) |
Hello. There are some solutions in thisthread.
|
11/26/2013 3:45 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (172)
|
Did you check this FAQ: http://support.automation.siemens.com/WW/view/en/61595882? |
Have Fun! |
|
11/27/2013 2:38 AM | |
Joined: 11/15/2012 Last visit: 8/29/2024 Posts: 143 Rating: (8) |
I update Step 7 to 5.5 sp2, it seems that this occurs less offen. I did the work by the linked guide. It is better, less annoyed,thank you. |
This contribution was helpful to1 thankful Users |
Follow us on