12/10/2013 7:25 PM | |
Joined: 12/27/2006 Last visit: 4/25/2024 Posts: 1196 Rating: (113) |
Yes, its easy to do. Firts count the pulses on the input to a counter. Do it 1 x per sec. With the value of the counter you make the caculation, zb x60, and reset the counter. Then you have the revolutions (impulses) per minute Attachmentrpm.zip (600 Downloads) |
12/10/2013 9:14 PM | |
Joined: 12/27/2006 Last visit: 4/25/2024 Posts: 1196 Rating: (113) |
Yes thaths also possible. First you have to VM mapping the value u want to show on the panel. Go to Toots > Parameter VM Mapping and make the rigt settings. In this programm, thats exact the same as before i have do it for you. In WIN-CCyou can programm this value (in the varable list) and set in on your panel Attachmentrpm.zip (346 Downloads) |
Follow us on