Industry Online Support
Technical Forum
8/11/2007 3:32 PM | |
Posts: 122 Rating: (4) |
picture
AttachmentPICTURE.zip (593 Downloads) |
8/12/2007 11:45 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi Peters, When declaring the DP/DP-Coupler you can choose between several blocks, when chossen then it is after that not possible to change it. So you can choose no bits, but bytes and words and the consistency have to be taken into account. See also the FAQ: What are the special features of input/output addressing with the DP/DP coupler? And also the Handbook: DP/DP Coupler |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on