Industry Online Support
Technical Forum
1/3/2014 8:34 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hello Raffy, The CPU 315-2EH13 has a work memory of 256 kbyte. The MMC should be one and a half time bigger to use the complete workmemory. So you can use a MMC of 512 Kbyte. When you want to store more files on the MMC, you need a bigger one. See the following link: S7-300: How can I find out the size of the MMC so I can store my whole STEP 7 project on it? And when you want to perform a Firmware update, you will need a 4 MB MMC Operating System Updates for CPU 315-2 PN/DP Best regards, Wizard |
This contribution was helpful to2 thankful Users |
1/22/2014 1:23 PM | |
Joined: 8/20/2011 Last visit: 4/12/2023 Posts: 22 Rating: (0) |
HiRaffy, You can choose above 4MB MMC card firmware update. Thanks DINESH
|
Follow us on