1/30/2014 1:48 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Hussain; The ports on the S7-200 are all RS-485, and the USS protocol uses this RS-485 interface. So you will need a RS-485 to RS-232 converter to connect to your drive on RS-232, if you are sure it uses the USS protocol (I have never seen it used on RS-232, myself). And the USS protocol ios dedicated to drive control, not for communication with PLCs. Have a look at the description of the USS protocol: Specification: Universal Serial Interface Protocol USS Protocol Would you mind giving us some information on these PLCs, maybe someone here has experience with them. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/31/2014 12:56 AM |
|
Follow us on