Industry Online Support
Technical Forum
2/3/2014 6:42 AM | |
Joined: 4/6/2009 Last visit: 3/27/2024 Posts: 10 Rating: (0) |
Dear Parshan, Unfortunately the ASM 475 cannot be configured in TIA Portal as no HSP is available. To configure the RFID system in TIA portal you can only use RF120C, ASM 456 or RF 180C. And for the above communication modules you can either use the new Ident Profile blocks or you can migrate the FB 45 blocks from Simatic manager to TIA portal. Refer the below link for more detail. http://support.automation.siemens.com/WW/view/en/77467630 As for as the reply for your question, you cannot use the ASM 475 in TIA portal (Neither on the S7 300 main Rack or in ET 200M racks). You have to wait for the HSP and the new firmware update. Regards Suresh |
This contribution was helpful to1 thankful Users |
2/4/2014 4:22 PM | |
Joined: 10/1/2013 Last visit: 4/17/2024 Posts: 605 Rating: (71) |
Don't forget RF160C ;) |
This contribution was helpful to1 thankful Users |
Follow us on