5/4/2012 9:06 PM |
|
Joined: 2/16/2011 Last visit: 4/4/2024 Posts: 229 Rating: (27) |
Hello; It really works. Regards
|
Gabriel de Oliveira |
|
5/5/2012 1:23 PM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046) |
Hello ace_sinergize as everyone already said, you will be just fine running the two Ethernet protocols together on your S7-1200. The only thing I like to add is that the HMI will actually NOT use Profinet (IO) commmunications, but instead S7 communications (its Siemens propietary protocol but utilises TCP/IP). I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
5/5/2012 5:15 PM | |
Joined: 5/17/2010 Last visit: 2/21/2022 Posts: 80 Rating: (1) |
Ok, thanks everyone for your help. |
2/7/2014 7:42 AM | |
Posts: 340 Rating: (6) |
new question is splittet to S7-1200, configuration profinet port, sample program, ethernet switch. |
Follow us on