2/12/2014 11:19 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello Ziemens As asvised by S7 AUTOMAN , we must use STEP7 V5.5+SP2+HF to solve this problem. However I cannot downgrade STEP7 installation from SP3 to SP2 as some of the softwares and modules will work only if SP3 is installed. So the problem still persists. I hope that Siemens issues a Hotfix soon to address this issue. Cheers Navnag |
Last edited by: Navnag at: 2/12/2014 11:23 AMThere is no such thing as the last bug in a program |
|
Follow us on