3/10/2014 9:04 AM | |
Joined: 6/20/2011 Last visit: 9/11/2024 Posts: 77 Rating: (7) |
This did the trick for me, as Windows OSK also is slow. http://social.technet.microsoft.com/Forums/windows/en-US/0bc87226-c064-49b4-a519-aac91a5c774c/slow-onscreen-keyboard-start?forum=w7itprogeneral I added netsh winhttp set proxy proxy.microsoft.com With Command prompt. |
Last edited by: GrasserF at: 3/10/2014 10:05 AMlink edit Last edited by: Rivas at: 3/10/2014 9:09 AM |
|
3/14/2014 10:23 AM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
Hello Rivas, The solution which worked for you sounds similar to that of the below mentioned FAQs. I am going to try out the same, shall post the feedback once I get through. How can you speed up the opening of the "Onscreen Keyboard" with SIMATIC IPC277D? |
Like it? Rate it! |
|
3/17/2014 7:51 PM | |
Joined: 6/20/2011 Last visit: 9/11/2024 Posts: 77 Rating: (7) |
Indeed looks too be the same issue. i also think the Advantech is running : Microsoft Windows Embedded Standard 7 |
Follow us on