4/3/2014 9:06 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hello Mr Khan, You can use a FM350-1 or FM350-2 (depends on frequency of counting): Here are some links with technical information: 6ES7350-1AH03-0AE0 SIMATIC S7-300, Counter Module 6ES7350-2AH01-0AE0 FM350-2, Counter Mod. 8 Channels, 20 KHZ Best regards, Wizard |
4/3/2014 9:49 AM | |
Joined: 4/24/2006 Last visit: 5/8/2024 Posts: 8638 Rating: (1151) |
Hello, Yes, you can use them with ET200M. Here is a link to manual: SIMATIC Distributed I/O device ET 200M See chapter 1.4 Best regards, Wizard |
4/3/2014 10:01 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi Mr Khan In the first post you talk about IM 153-1 and then write the code for an IM 153-2 have a look: SIMATIC ET 200M Interface Modules - Distributed I/O ... - SiemensTechnical data
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Last edited by: Ste39 at: 4/3/2014 10:06 AMLast edited by: Ste39 at: 4/3/2014 10:04 AM |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
This contribution was helpful to1 thankful Users |
4/3/2014 11:55 AM | |
Posts: 40 Rating: (0) |
kindly suggest the module for this with order code ... |
4/3/2014 11:58 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi If you have IM 153-2 look at first post of Wizard |
Follow us on