8/24/2009 1:37 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Dear Ahmed Ganainy, Perhaps the following links might help: http://support.automation.siemens.com/WW/view/en/16650737 /tf/WW/en/Posts/16691#top Best regards, Wizard |
This contribution was helpful to1 thankful Users |
8/24/2009 3:36 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hi, Are you using Software redundancy? Perhaps this manual is useful: http://support.automation.siemens.com/WW/view/en/1137637 See chapter 5.3 Best regards, Wizard |
8/25/2009 10:26 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Hello Ahmed, Are you sure you have this part number in picture? You say it's a new installation so it sounds very strange to me because this module had already entered cancellation phase in 2004. Best regards. H-H |
8/26/2009 10:39 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Hello Ahmed,
I still recommend to make sure of the part number andthe wholehardware configuration. Still, this part number (6ES7 153-2BA00-0XB0)had entered cancellation phase 3 years ago. So, please make sure you have this part number because if you ordered your IM couple of years ago you would have got 6ES7 153-2BA01-0XB0 and if you ordered your IM in 2008 you would have got 6ES7 153-2BA02-0XB0. It is always better to have hardware in your office/lab to make enough measures and tests. You need to test switching over of CPUs, IMs, HMIand data transfer time between the 2 CPUs. Imho 30 mins is a tight time for this. Software redundancy is not an easy solution and it hardly runs from the first shot. I think more members can offer more help if you upload your hardware configuration to check if it's proper for software redundancy or not.your configuration islittle vague in the picture. Moreover, we can check software redundancy parameters if you upload your software. This is just to make sure that it should run trouble free in site. Best regards. H-H |
This contribution was helpful to1 thankful Users |
4/9/2014 5:43 PM | |
Joined: 7/26/2009 Last visit: 8/28/2023 Posts: 16 Rating: (0) |
dear H-H Hi I attached the project. AttachmentSwr_30_1.zip (99 Downloads) |
Last edited by: sina20795 at: 4/9/2014 5:49 PM |
|
4/10/2014 6:24 AM | |
Joined: 7/26/2009 Last visit: 8/28/2023 Posts: 16 Rating: (0) |
please see the attachment picture |
Follow us on