Industry Online Support
Technical Forum
3/22/2012 3:51 PM | |
Posts: 467 Rating: (59)
|
hello, there are three possibilities to insert SIMOCODEpro to the STEP7 HWConfig: 1)by GSD file: SIMOCODEproC: it's possible to set all SIMOCODEpro parameters at GSD file. -> If parameter "start-up parameter block" is disabled at SIMOCODEproC,it will get this GSD parameterization at start-up SIMOCODEproV: parameterization must be done by SIMOCODE ES stand-alone Download: PROFIBUS GSD files : SWITCHGEARS (see Station type: SIMOCODE pro C / SIMOCODE pro V) http://support.automation.siemens.com/WW/view/en/113630 proC: SI0180fd.gs* proV V1.3: SI1180fd.gs* proV V1.4: SI1280fd.gs* (with new DM-F PROFIsafe module) 2)bySTEP7 Object Manager for SIMOCODEpro(SIMOCODE ES Premium integrated to STEP7) thisSTEP7 Object Manager (OM) is coming with SIMOCODE ES Premium, You have to choose this option while setup. With STEP7 Object Manager you can use SIMOCODE ES software integrated to STEP7 HWConfig to store parameterization at DP-Master (similar to GSDfor proC) andyou have the userfriendly SIMOCODE ES software environment and this can be used for proC and proV. Also "start-up parameter block" must be disabled to receive the parameterization stored at DP-Master at start-up. See following restriction on number of devices per DP-Master system: 3) by SIMATIC PDM (common for PCS7 environment) With SIMATIC PDM and the SIMOCODEpro EDD fileit's possible to parameterize SIMOCODEproC and proV. After saving, compiling and download to SIMATIC S7 the communication between PLC and SIMOCODEpro devices is running (dont' forget to assign PROFIBUS address to SIMOCODEpro devices!) Cyclic Send / Receive is done by I-/Q-Adresses given at HWConfig for the device. Here a sample programming for acyclic communication (Read/Write data set)
kind regards LesPaul AttachmentSFC 58 & 59_Simocode Pro.pdf (638 Downloads) |
This contribution was helpful to3 thankful Users |
4/23/2014 4:14 PM | |
Posts: 12 Rating: (0) |
hello pathers, your posted were great help, but i dont can see datarecord, my cuestion if i need extra configuration another parametrer in the simocode ES, for i'll can not see the dtarecord Saludos AttachmentDP_6.zip (387 Downloads) |
Follow us on