Industry Online Support
Technical Forum
12/19/2005 2:10 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, you can not use AS511 with the CP523. (Only FAP) The best are you use a IM 308-C (Profibus) For this you need Com-Profibus Software. but notes: It isa old IM and Software and did not know, if you can bay it yet. In the internet i found the following FAQs For the communication with IM 308C an a CE- Panel look to the chapter 4. There are all described what you have to do -> FBs and so on. http://support.automation.siemens.com/WW/view/en/1405528 The other FAQ will be also very helpfull. http://support.automation.siemens.com/WW/view/en/17053153 http://support.automation.siemens.com/WW/view/en/22117386 A other way will not be possible. (If you use a S5 155U and CPU948) |
Follow us on