5/23/2014 10:47 AM | |
Posts: 12 Rating: (0) |
Hello I've got a problem with a S5-S7 conversion. The problem is that i have a Central Module CM-10-SSIwith adaptation capsule also inS5-115U ( my CPU is 944/115U- 6ES5 944-7UB22) and for the S7-300 i don't know what card i need to replace the old one (Central Module CM-10-SSI), the new CPU is6ES7315-2EH13-0AB0 (SIMATIC S7-300, CPU 315-2PN/DP) and i upload the data sheet of Central Module.Any body can help me tu replace that card????
Thank you AttachmentCentral-Module CM-10-SSI.pdf (241 Downloads) |
5/23/2014 11:35 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181)
|
What is connected to it? What kind of application is? |
5/23/2014 12:01 PM | |
Posts: 12 Rating: (0) |
There are connected two absolute encoders,CE-65-M SSI and LA-41-SSI, i upload a JPG with the connection of that encoders at the card. |
5/23/2014 8:10 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello Duma You need : 6ES7338-4BC01-0AB0 - SIMATIC S7-300, SSI SIGNAL. MODULE SIMATIC S7-300, SIGNAL. MODULE FOR 3 SSI SENSORS FOR READ-IN OF POSITIONING VALUE WITH 2 FREEZE INPUTS , 1 X 20 PIN, SUPPORTS ISOCHRONE MODE The Module supports 3 SSI Encoders, Manual is attached below Hope this helps Cheers Navnag AttachmentSM_338_SSI_Module.pdf (261 Downloads) |
Last edited by: Navnag at: 5/23/2014 8:14 PMManual Attached Last edited by: Navnag at: 5/23/2014 8:11 PMThere is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
5/23/2014 8:41 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
I Noticed one problem though ... the SM 338 SSI Module only supports 13 /21 / 25 bit SSI Encoders. While the S5 Module you are referring to supports 24bit SSI Encoders. I am not sure if 25 bit SSI setting on SM 338 will work for a 24 bit SSI encoder. However you can use ET200S SSI Encoder Module : 6ES7 138-4DB03-0AB0 in a ET200S Rack. It supports : 13/14/15/16/17/18/19/20/21/22/23/24/25 Bits !! Here are the Details of : 6ES7 138-4DB03-0AB0 SIMATIC DP, ELECTRONIC MODULE F. ET 200S, 1 SSI 25BIT/1MHZ 15MM WIDE MODULE FOR CONN. OF ABSOLUTE ENCODERS WITH SSI INTERFACE SYNCHRONOUS SERIAL INTERFACE WITH DI AND COMPAR. VALUE WITH CLOCK CYCLIC SYNCHRON. APP Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on