Industry Online Support
Technical Forum
5/5/2012 9:43 AM | |
Joined: 12/20/2010 Last visit: 4/2/2024 Posts: 21 Rating: (0) |
Dear Nikzitronik, Thanks for your response. Actually my plan is not adding three CM DP-Master on the main master PLC. My plan is to divide the 30 slaves into 3 groups, and each group has one sub-master. Each sub master has the following: - Slave CM DP to communicate with the main master PLC - Master CM DP to communicate with the reset PLCs in the group. Then the data in slaves will be transfered to sub masters first, them the sub masters will transfer the data to the main master. Please see that attached file to see the system overview and the suggested NET config. Waiting your openion Attachment30 Slaves of S7-1200 NET.pdf (223 Downloads) |
5/26/2014 11:20 AM | |
Joined: 4/21/2006 Last visit: 4/16/2024 Posts: 510 Rating: (24) |
New question was splitted to a new thread: S7 300 (S7 1200) connect with 23 remote stations. |
Follow us on